STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

S2LP WMBUS SMPS VOLTAGE

Hello;My Name is FATIHI am using Wireless MBUS water meter scanning using S2LP and STM32L073. While making the PCB design, we applied the reference design value in the x-nucleo-s2868a2_schematic.pdf file exactly. However, although we see VDD voltage ...

FATIH55 by Associate
  • 1190 Views
  • 1 replies
  • 1 kudos

BLE P2P connection problem.

HiI am using USB DONGLE board (MB1293C) as client and Nucleo board (MB1355D) as server.The BLE_p2pClient application is downloaded in a USB DONGLE board and the BLE P2P_Server application is downloaded in a Nucleo board.My problem is that most of the...

YasinYelkovan_0-1718881097762.png

Resolved! STM32WB ADC not working along with BLE

Hello, I am trying to read battery voltage within a task called by sequencer on STM32WB55CEU.I am following this post: https://community.st.com/t5/stm32-mcus/how-to-use-the-stm32-adc-s-internal-reference-voltage/ta-p/621425I verified that I can measu...

mx1.png a4d5ed2f-c2e3-47ee-b054-d171b82f8b44.png mx2.png

Resolved! B-L072Z-LRWAN1 LoRa Receiver Rate

Hello, I am using B-L072Z-LRWAN1 in a project. I have one board acting as a transmitter and 3 boards acting as receivers. My question is: Is it possible to transmit and receive with a rate of 5kHz with is every 0.2ms a 30 byte payload using LoRa? 

Sondos by Associate II
  • 1539 Views
  • 1 replies
  • 2 kudos

Resolved! Ping pong example not working on STM32WLE5CCU6

Hello, so I am using two RAK3172 and trying to run SubGHz_Phy_PingPong example as it is, but it is not working This is the log on both end, I attached the screenshot of one device, I also tried by doing iq inversion on both the devices, but it's stil...

pho3nix_0-1720518585320.png
pho3nix by Associate III
  • 1827 Views
  • 1 replies
  • 0 kudos

se-identity.h

I have a node connected to a gateway and a chirpstack server.  I decided I want to understand a few topics.  So I went into the above file and changed the EUI from a working 80,00,00,00,00,00,00,06 to below. #define LORAWAN_JOIN_EUI ...

SWenn.1 by Senior III
  • 1291 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55 BLE Unexpected Event

I got the STM32W55 MCU.We keep receiving an event from the stack:Event type: 0xff -->   HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE  Event e-code: 0x04   /* ACI_HAL_END_OF_RADIO_ACTIVITY_EVENT code */ #define ACI_HAL_END_OF_RADIO_ACTIVITY_VSEVT_CODE ...

ezza23 by Associate
  • 2165 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.