STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55CG I2C MASTER COMMUNICATION FAILURE

 Hi,I'm trying to read battery information from a BMS chip (I2C slave) via I2C.  And I also tried to capture the clock signal on SCL with scope but it failed.  This chip is already used in our other project with another MCU.  This is my first time to...

I2C_Registers.PNG
DFeng.2 by Associate II
  • 1245 Views
  • 1 replies
  • 0 kudos

Bootloader not working on STM32WB5MMG

Hi, I have a product with 2 microcontrollers on the same PCB(running independently). One is STM32G030 and other is STM32WB5MMG(ble module containing STM32WB55). I enabled internal bootloader(via option bits configuration) for both the microcontrolelr...

KlemenDS by Associate II
  • 1925 Views
  • 3 replies
  • 0 kudos

Resolved! Low Throughput on STM32WB1MMC

I have setup a client and server with two STM32WB1MMCs and have the server periodically send data based on a frequency stated by the client. My payloads are 10 bytes long and are incrementing values for me to keep track of any losses. I am finding th...

JacobFA by Associate
  • 989 Views
  • 1 replies
  • 0 kudos

STM32WB55 Bluetooth Issue

Hello Dear Person,We already work with STM32WB55 and sometimes Bluetooth didn't make a advertising. (same software works another STM32WB55 without problem.) CPU already run without problem and make all works to do.Which issue cause that issue?How can...

Resolved! STM32WB55 Ble Configuration

Hi, I am using the STM32WB55CCU6 base custom board. In that board i am not using LSE crystal oscillator (32.768Khz). Is it possible if i can run my BLE application without the LSE?Please provide your suggestion in as soon as possible. Thanks in advan...

ksaini by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

BLE Operation in Low Power Modes on STM32WB

Hi,I'm not sure if I fully understand how the low-power mode works with active BLE on the STM32WB. I have an application using FreeRTOS and the BLE stack. I have set up advertising and am able to send and receive data over BLE. This works fine. When ...

JR2963_0-1726493511723.png
JR2963 by Senior II
  • 2503 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.