STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Follow Up webinar on STM32WB0 MCUs

Hello,This message is for ST team.I attended the webinar on STM32WB0 MCUs, but I didn't receive the e-mail that was supposed to follow, including the links, recording and voucher for the demonstration board.What happens ?PS: I'm posting here because ...

Doom by Associate
  • 1622 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5 SubGhz Debug - Alternate functions

Hi , in the Datasheet there are few interfaces which are marked as "alternate functions" for DEBUG_RF or DEBUG_SUBGHZSPI.  ( Table 20 in the Datasheet)But , I didnt find any info regarding what can I use those function for ? for example - Can i acces...

viola by Associate III
  • 2108 Views
  • 5 replies
  • 1 kudos

Zigbee connection control

Hello, I have configured a Zigbee network using an STM32WB55 MCU with 1 coordinator device and 5 end devices. However, since I cannot check whether the Zigbee connection is lost or not, I am resetting the end devices every 1 minute using NVIC_SystemR...

oarslan by Associate II
  • 3622 Views
  • 10 replies
  • 0 kudos

Resolved! STM32WB55CG Zigbee LED Controller (Color)

Hi,I have used a custom board with an STM32WB55CG MCU to successfully connect to a Tuya Gateway and also a Homassistent/Zigbee2mqtt setup with the OnOff functionality.As next topic I wanted to add a color control functionility and tried several optin...

vh789 by Associate III
  • 4227 Views
  • 5 replies
  • 2 kudos

About STM32WBA products support EPA?

Hi all,I check with STM32WBA55 datasheet have description can supported external PA.   But FW SDK(STM32Cube_FW_WBA_V1.4.0) released notes exist below description.  It look Known Limitations is not support EPA, usually need logic control between FEM a...

EthanChen_0-1727395726894.jpeg EthanChen_1-1727395753052.png
EthanChen by Associate II
  • 1585 Views
  • 2 replies
  • 0 kudos

Resolved! Use the DMAMUX with SUBGHZSPI_TX (STM32WL55 or STM32WLE)

Hello,First of all, a short text in order to present my problem :After reading all documents about the STM32WL55 and STM32WLE concerning the SubGhz and DMA, I don't find how can I use the DMA and DMAMUX with SUBGHZSPI_TX.Furthermore, I'm working on t...

Capture d'écran 2024-09-18 103719.png Photo.png
SamirDB by Associate
  • 1303 Views
  • 1 replies
  • 0 kudos

Resolved! What is the output impedance of the STM32WB55?

I check the datasheet and it say that the output impedance os the STM32WB55 is 50 ohms , so i don't must need impedance matching but on the reference design have a pi-match circuit and a RF filter. Really the MCU have a 50 ohms impedance output or th...

0693W0000058ub9QAA.png
0x34 by Associate
  • 6393 Views
  • 9 replies
  • 0 kudos

Resolved! STM32WL: TCXO series impedance calculation

Hello,I'm planning to use an STM32WL5X microcontroller in an upcoming project, and I found myself confused on the recommended impedance for external 32MHz oscillators. Please see the attached image for a screenshot from the datasheet.The datasheet sa...

AJ_1 by Associate III
  • 3639 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.