NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear ST Support Team,I am working on a project using the STM32WB5MM module, where I am trying to create a custom BLE service under Server mode, and also enable FreeRTOS for task management. However, I’ve encountered an issue where the Custom Server ...
Hi there.I'm trying to use the STM32WB0 (NUCLEO-WB09KE) in HCI Controller mode with our Bluetooth Stack: https://github.com/bluekitchen/btstack/I found the BLE_Transparent application in the STM32WB0 Firmware package which provides HCI over the virtu...
I've found something curious in the code generated by CubeMX for a BLE application on STM32WB. In APP_BLE_Init we have this:/** * Do not allow standby in the application */ UTIL_LPM_SetOffMode(1 << CFG_LPM_APP_BLE, UTIL_LPM_DISABLE);My understandin...
How to erase STM32WLE5JC so that I can put my binary in the Seeed Studio Wio-E5 module. Web says changing the lock bit from hex value of ??? to ???. Where can I set it? TIA
Hello STM32 community, I'm currently working on implementing Zigbee applications on my STM32WB55 Evalution boards, and I'm looking to create custom clusters. I've gone through the documentation custom-clusters, but I'm a bit confused about the proce...
Hi,I'm working on implementing attribute reporting on the Zigbee STM32WB55 Evaluation boards. I've attempted to configure attribute reporting in the Zigbee_DevTemp_Server_Coord and Zigbee_DevTemp_Client_Router baseline examples. However, I encounter...
I've been having a lot of trouble getting all of the online BLE examples to work and was hoping someone could steer me in the right direction. In every example they state that the RFWKP Clock Mux should be set to LSE but whenever I do that the main ...
Hi , I see in the Datasheet in Table 31 some reciever parameters .I need to know what is the Dynamic Range of the Reciever in the STM32WLE5 . can you point me to which parameters should I look at ? Thank youViola
hi, I have two B-WB1M-WPAN1 cards and I would like to create a program that works as a client server, so one card will act as a server and then other client cards will send messages to it via BLE, I saw the example proposed by the company "BLE_HR_p2p...
Hello, I have a question regarding having both library (from the example files) SubGHz and LoRaWAN on the same microcontroller STM32WL5MOC at the same time and my idea is to use a switch to choose which on i would like to use depending in the case of...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.