NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Is support for the nucleo-wb15cc already in Zephyr or does it need to be added? I am new to zephyr and would like to avoid re-inventing the wheel if possible. From a setup I just created today (so should have the latest released code) I didn't see t...
Upon triggering a notify event calling the following function "Custom_STM_App_Update_Char()", the STM32 successfully sends data, which I receive on my iPhone using ST BLE Toolbox. However, after that, the STM32 becomes unresponsive to further BLE req...
Hi, I developed an application using the stm32wb5mm-dk. Everything works until I try to use an external 5V power supply. In fact, I change the position of JP2 on position 7-8 (to select 5V EXT) and I soldered SB4. However, when I supply the board thr...
Hi,i am working with BLE_p2pServer_ota example as a template and i want to send 5 Bytes of data from the client (nRF Connect App on the cellphone) to the server (NUCLEO-WBA55). However, I am having trouble receiving more than 2 bytes.1. I made a new ...
Hi,in my low-power STM32WL55 application I would like to use the LPUART to receive data (no transmission) while the device is in STOP2 mode. I have two questions about this:The reference manual states:"Before entering low-power mode, make sure that n...
Hello... Here I am developing a battery based IOT-STM32 based project and I am unable to read and write ADC using this new chip STM32WL5MOCH6S. Please provide me any detailed document related to ADC or Any kind of example code which I can check in my...
Hi, I am developing on the Nucleo-wl55jc2 development board and I am trying to program the sub-GHz radio to transmit a continuous wave (not sending data packets, just a waveform). I have attached my code below along with a zip of the project. This ...
I m using stm32wle5jci6 i am getting stuck, device is not sending join request. And i m new to this so not able to understand what us wrong. ###### AppKey: 2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3C###### NwkKey: 2B:7E:15:16:28:AE:D2:A6:AB:F...
I'm trying to use STM32WB09KE for the BLE application. However, unlike STM32WB55, this microcontroller must activate PKA and RNG for the BLE module.So, I did.However, after generating the BLE code, I tried to build the project in the IDE and it showe...
I am trying to familiarise myself with the thread using the wiki page STM32WB_OpenThread_Border_Router_Application and am not getting anywhere because some graphics are missing on the page and I especially need the graphic with the CLI commands. It i...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.