NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi Community!Currently working with the STM32WL5MOC module on my custom board.I'm trying to work with the ADC but getting values like the fallowing and not changing even when i connect the ADC signal to ground. light: 1366light: 1367light: 1367light:...
Hi,i use the example ble_p2pServer_ota with STM32WBA55. How can i send a value (uint_8 or a string) from the server (NUCLEO-WBA55) to the client (Cell Phone)?Here in the example code (file p2p_server_app.c), the value of Switch_c_NOTIFICATION_ON for ...
Hi,I am working with the ble_p2pServer_ota example with an STM32WBA55 controller.If I want to send data (one byte for example) to an app on a cell phone, what settings do I have to make in the characteristics in CubeMX?
Hi ,Regarding working with the STM32WLE5 with SUBGHZ block in the CUBE-MX.in the clock section tab in the CUBE-MX I dont see any mention of the RF-PLL clock. if i understood correctly - in order to work with the LORA SUB-GHZ BLOCK i need to supply a ...
Hi,I am using Zigbee_OnOff_Router_NVM to test the opening and closing function of IasZone Server. I found that by default, the notification generated by modifying the status value is 'Report Attributes'. But according to document 'Zigbee Cluster Libr...
I tried loading the p2pserver_ota example binary at address 0x08004000 and before that I flashed the application manager at address 0x08000000.When I reset the controller I get these logs at usart1 and my led2 connected to pb11 starts blinking-==>> S...
Hi,I hope everyone is fine.I have question about Inheritance Certification.The Thread Group says;The Thread Group allows certification by inheritance for families of end products that reuse the same Thread system (chip and stack) and the same use cas...
Hi,i am working with NUCLEO-WBA55 and using the BLE_p2pServer_ota example as a template for my project.Unfortunately, the program does not start when I supply it with power via USB but only after I have pressed the Reset button. Can someone please he...
Hello,I have an STM32WB and I am trying to get the data from some pressure, temperature and humidity sensors through DMA and send them to my Android via BT, while at the same time saving it as well on a SD card with SPI. Both programs work quite well...
How to port BLE Mesh Lighting application SW for BNRGLP into STM32WB09?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.