NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello everyone,I want to try to wakeup my system from the the STOP2 mode with a button press. The button is also in use in the rest of the application and works just fine. But when going to STOP2 it does not wake up the system again.I've tried it wit...
I think it is the most popular topic among STM32 programmers who use ST-LINK V2 programming devices.I have two devices: one is the Lora E5 MIni, and the second is the Lora E5Dev board. Both respond to the AT commands, so I expect they are healthy.A f...
I am trying to upload BLE stack on my custom designed board. The MCU is STM32WB35CCU6A. Below is FUS Version, I am able to get from MCU. but when I try to upload BLE stack , I see below error. Error: FUS_STATE_IMG_NOT_FOUND: Firmware/FUS upgrade req...
Hi, I'm developing my custom board using STM32WB09TEF7TR Microcontroller but have a problem during Programming using STM32cubeIDE. I can access the memory of this microcontroller using STM32CubeProgrammer through SWD protocol.However, once I try to ...
Hello,I have used to read EXTI.SWIER1 to know if interrupt comes from SWI or external. But it seems that WB55 doesn't allow to read anymore the SWIER1 register. The RM notices that reading SWIER1 returns always '0'.So my question is : How to know the...
Hi everyone,I am currently working on the LoRaWAN_AT_Slave example from the firmware package repository (STM32Cube_FW_WL_V1.3.0) provided by ST. So far, I have successfully implemented uplink and downlink communication, enabling the device to send se...
I am in a similar situation to @Richard Lowe back here:https://community.st.com/t5/stm32-mcus-wireless/looking-for-uart-guidance-for-the-stm32wb05kn-network-co/m-p/721231The getting started guide from the last post there references a "X-CUBE-WB05N us...
Hi. I`m using Zigbee_OnOff_Router_NVM example on WB55CGU6 custom board with existing Zigbee network in my home, but seems that my device not act as router. I mean that it not extends range of my network. What i do wrong?i checked:Set config.startupCo...
Hi. I have a problem with the STM32WB09KE board.I'm trying to activate Bluetooth LE using this developer board but the BLE init function returns this error massage. Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSETSuccess: aci_h...
Hi, I am using stm32wba55cg nucleo board, and running the example application BLE_p2pServer. While the serial logs of the board show that the device is in advertisement mode, it can not be discovered on my samsung s20 fe, running android 13.I tried u...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.