NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi to all!We are developing a low-cost application, with in mind STM32WBA52KE, which use a 32 pin package.Due to short number of pin, we would use pin 12 and 13 as GPIO, so we should not use the LSE.Is it possible to manage the BLE stack without LSE,...
Hi!I am trying to reproduce some examples and got stuck at simple sensor.The example code is working fine on my P-Nucleo-wb55, but if I am trying to reproduce i with CubeMX i've got failedCode is simply stuck at void shci_cmd_resp_wait(uint32_t timeo...
Hello, please, can I put the power antenna configuration to the maximum 8dBm? and how? thanks
I'm using the STM32WB55 for BLE communication with an Android device, starting from the BLE example HeartRate monitor with FreeRTOS. Sometimes, when I disconnect from the STM32 using my mobile, I don't always receive the notification callback on the ...
Hi,I'm currently working on a project using multiple B-WB1M-WPAN devices:one acts as BLE Central;the others act as BLE Peripherals.I'm using the STM32_WPAN software package in CubeMX 6.14.My question is: how do I create a Central that is able to inte...
Hello STM Community,I am designing an internal PCB antenna for LoRa communication using the STM32WL55JCI7 at EU868 frequency. Is a PCB antenna recommended by STM for this chip? If so, what guidelines or procedures should I follow for designing a PCB ...
Hello i'm starting programming with stm32, i've bought the stm32wb5mm-dk and with stm32cubemx I've tried to configure the board to create a ble ibeacon.So, now i can see the ibeacon from nrf app but isn't showed the name (N/A ibeacon). How can i see ...
Please let know how to change Connection Interval. I need to decrease Connection Interval value so data sampling frequency can be increased. STM32WB35 is working in peripheral mode. Thanks
I am currently experimenting with the LL data length extension feature on STM32WB55.I want to increase max TX length in link layer packet.I would appreciate it if you could tell me how to increase max TX length.(Looking at the current LL_LENGTH_RSP p...
BLE_HeartRateFreeRTOS example.There is an event when someone writes to my characteristic.Is there an event when someone reads any of my characteristics?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.