NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I am trying to run micro python in Nucleo-68 STM32WB55R6VG.I followed the link https://docs.micropython.org/en/latest/develop/gettingstarted.html#building-the-stm32-portI am able to generate the binary files(hex,dfu,bin,elf)I flashed firmware.bin ...
Hello,ST experts I have read Wiki on https://wiki.st.com/stm32mcu/wiki/Connectivity:Introduction_to_LoRaWAN. And we want to build a LoRAWAN based on STM32WL series MCU. But it seems not very clear what is the performance of the LoRA gateway. E.g. 1km...
Hello.I'm using the Nucleo-WL55JC board with LoRaWAN End-Device firmware (US915 region).To measure the current consumption of the RF section, I removed the JP2 (I_RF) jumper (as per the manual) and connected an ammeter.The issue is that the RF sectio...
When I enter standby mode using HAL_PWR_EnterSTANDBYMode(), the program is expected to halt at __WFI() until awakened, after which it should restart from the beginning. The function is shown as followed. However, in my case, after executing __WFI(),...
When "Middleware and Software Packs" > STM32_WPAN is enabled in CubeMX, a duplicated initialization's code for uwTimclock is generated: That code is outside the if-else block overriding the previous configurations which could produce issues. Any ...
I'm trying to achieve a simple characteristic read from a client device on a STM32WB55 to a server device on a STM32WB35on client side - after connecting I get a HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE and I keep track of connection_handle in a grobal...
We are developing a product using the STM32WB55 chip and using the S.T W.P.A.N stack. We intend to release our product with a Bluetooth certification / logo, so we need to register our company to get a company I.D right ? Do we need to use the compan...
Dear I hope you are doing well.I would like to confirm if the default antenna power of the STM32WB05KZ board is set to 0 dBm ? Additionally, could you please guide me on how to modify this power setting?Thank you in advance for your support. I look ...
HelloI have a question, please. I am planning to use a Bluetooth module, and since I am required to apply potting, could you let me know which antenna is less affected by it: the chip antenna or the PCB antenna?thanks
I am using stm32WLE5CCU6 chip from ST, but I can't connect 2 chips together using lora. Can you give me sample program for this chip?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.