2022-12-08 8:02 PM
Hi
I just bought a B-L4S5I-IOT01A Discovery kit.
Confession: I am completely new to ST, and I reckon I have a mountain of learning to do in a short time.
However, I just read the blurb on the back of the kit and it essentially says:
1. Verify the jumpers are in the correct position
2. Connect to USB
3. Open terminal and enter Wi-Fi details
4. The loaded demo app will then connect to the Wi-Fi and the demo app will start an HTTP server.
Well, I did steps 1, 2 and 3 and waited. But every time I try, I get the following:
ERROR : es-wifi module NOT connected
The complete output is output was as follows:
Running HTML Server test
eS-WiFi Initialized.
eS-WiFi module MAC Address : **:**:**:**:**:**
Already configured SSID: *** (WiFi) security: 2
Press board User button (blue) within 5 seconds if you want to change the configuration.
Connecting to ****** (WiFi)
ERROR : es-wifi module NOT connected
2022-12-09 7:36 PM
Check the board sticker and compare the board version with the ones decribed in the board user manual.
Sometime the wifi module may need to be reprogrammed?
2023-02-14 8:06 AM
Hello
Are you using an iPhone as a WiFi access point ? recent versions of iOS offer WiFi hotspot with only WPA3 for authentication . B-L4S5I-IOT01A only supports WPA2. You should try with another WiFi access point (WiFi router).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.