2019-05-29 2:17 AM
Hi all,
Recently, I build a project with TouchGFX for STM32H743,and the total files are more than 2MB,so I have to use external flash memory(W25Q256).
Then, I am trying to use QSPI interface to connect external memory and execute in interrupt method.
But I have no ideal how to build the function,can any one help me or provide source code?
By the way, I have already added the algorithm about W25Q256,and the other initialize was done , backlight was turned on.
Thanks!
2019-05-31 12:57 AM
Yes, but I have already built a external flash algorithm for it.
And I found all the QSPI function at Community,there is no likely method.
Or do you have any suggest or reference code?
Thanks!
2019-06-13 6:07 AM
Hi @Charlie CHEN,
Did you get anywhere with this?
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.