2023-05-23 5:39 AM
When defining a fade duration of e.g. 350 msTouchGFX generates a tick time of 21 ticks based on the 60 Hz LCD update rate.
My LCD now had to be adapted to only have an update rate of appx. 30 Hz. Then the fade duration is double in time.
Is there a way to define the number of ticks which TouchGFX uses per 100 ms or maybe the LCD update rate, so the used number of ticks fits to the wanted time?
Thanks for any proposals.
BR GS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.