2023-05-22 9:54 AM
I found a nasty effect after generating code with TouchGFX designer (V. 4.21.4):
In my project there is an additional include path, which is located in a different location as the touchGFX project on drive C. Every time after generating code, the files which are located there are no longer found and I need to define that include path again.
The path entry however seems to be still in the list, but I have to enter the path explicitly and simply pressing ok does not help.
The name of the path is (maybe this information helps to find the problem):
C:\Eigene Dateien\Projekte\ARM\Project\xProTT_Common\Inc
Maybe I will have to move the files because I need to regenerate code very often from now on for the project...
Any help or idea very welcome!
2023-05-22 11:24 AM
Hello. I would test to remove spaces on this include file path. Tgfx cannot handle spaces at least in the project folder path.
2023-05-23 5:33 AM
Yes, I know that the blanks in the project path are not allowed.
I moved my folder for the common parts into the TouchGFX project. This works now for me.
Renaming the original folder "C:\Eigene Dateien" is not possible as there are too many references which have to be kept for other projects.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.