STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How it works the return??

Hello all,I'm using the HAL library for the camera, specifically I'm using the function: HAL_StatusTypeDef HAL_DCMI_Start_DMA(DCMI_HandleTypeDef *hdcmi, uint32_t DCMI_Mode, uint32_t pData, uint32_t Length)In the function are many return HAL_ERROR, an...

BTurc.2 by Senior
  • 3327 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFXDesigner without Internet or on linux

My company has strick internet security. So TouchGFXDesigner is not connected to the internet. Can I use TouchGFXDesigner without Internet?So there is another PC installed Linux. Internet security for Linux is not very strict. If possible, I want to ...

sini by Associate II
  • 1952 Views
  • 2 replies
  • 1 kudos

DSI display interface doesn't work

HiI'm development a board with STM32F779a cpu connect with dsi display.I create the graphic wit TouchFX tools and included in the STM32cube ide design software.How example I see STM32f769i-disco demo, and received the init code of display by producer...

PZamb.2 by Associate III
  • 11794 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.