2021-06-25 12:55 AM
Hi everyone,
I have a button (flexbutton), that should triggers a different action depending on his previous state. For instance, my button should light on or light off a light, depending on his previous state. If the button was previously activated, it switchs the light off, and vice-versa.
In WPF I used a proprety called "tag", which was changing depending on the user actions, but is such thing or similar available in TouchGFX ?
I don't want to use toggle buttons, multiple buttons or create a variable in code.
Thanks!
Solved! Go to Solution.
2021-06-25 4:47 AM
Sorry, but you have to write this code. Flex button doesn't keep own state like Toggle button does. I would suggest to use C++ member inside View class. Or you can use Toggle button with other bitmaps if you do not like existing ones (designer has some styling options).
2021-06-25 4:47 AM
Sorry, but you have to write this code. Flex button doesn't keep own state like Toggle button does. I would suggest to use C++ member inside View class. Or you can use Toggle button with other bitmaps if you do not like existing ones (designer has some styling options).
2021-06-25 7:18 AM
ok thanks, good alternative, hope a tag feature will come in the next release!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.