STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Tearing effect happens randomly after reboot

STM32H750 with external flash and SDRAMTouchGFX version: 4.13.0CubeIDE version: 1.3.0display size: 480x272(landscape), but I config the display orientation in portrait in TouchGFXcolor depth: 24bitshttps://drive.google.com/file/d/1zCucWuLi5BSJUm0VCHa...

JLee.32 by Associate III
  • 2859 Views
  • 6 replies
  • 0 kudos

Resolved! How rotation works in texture maps?

Hello; I try to undestand touch gfx watch application. I could not understand how the pressure arrow is rotating without any interaction algorithm. Is the rotation of texture map related with orego? What makes the 2 step forward and 1 step backward, ...

limit_SKY by Associate II
  • 3381 Views
  • 4 replies
  • 0 kudos

ListLayout child container height changed problem

I am having issue to display a keypad container inside ListLayout. Problem: After displaying the keypad container by setting the container height, and invalidating the container & ListLayout, the other child inside ListLayout is not moved shifted/rea...

0693W00000BbsF9QAJ.png 0693W00000BbsKDQAZ.png 0693W00000BbsKhQAJ.png 0693W00000BbsLLQAZ.png
Xxoyo.1 by Associate III
  • 835 Views
  • 0 replies
  • 0 kudos

SPI2 in stm32f429 is not working while touchgfx and lcd config functions are added, however works fine if i comment the lcd config function and touchgfx init.

The lcd configuration uses LTDC(for data) and SPI5 for sending commands. The display driver used is ili9341. system clock configuration is as below./** * @brief System Clock Configuration *     The system Clock is configured as follow : *      System...

Eivor by Associate II
  • 2159 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.