2021-02-05 10:42 AM
Have anybody QSPI loader algorythm for Keil?
I can't create workable code....
Solved! Go to Solution.
2021-02-06 10:14 AM
I changed pins to my board and changed 4-byte mode to 3-byte mode.
QSPI initialising, memory_mapped_mode starts, but all readung bytes are "0x88"....
Same settings in main project works good....
2021-02-06 10:50 AM
0x88 is indicative of the flash part not being in QUAD mode, or command being wrong (unsupported, inconsistent with current mode, etc)
Would recommend doing a JEDEC READ ID, of one then both chips together (interleaved)
2021-02-07 5:36 AM
Thanks! Everything works! There was an error in the GPIO settings - I changed the numbers and ports, but did not change the parameters (AF9,AF10).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.