2025-03-18 8:41 PM
Would it be possible to add the Radio Button capability to the Flexbutton?
2025-03-20 2:58 AM
Hello @PSpectrum,
It's supported by changing the trigger type to "toggle", please refer to the documentation Flex Button | TouchGFX Documentation.
There's also an example showing that.
Best regards,
2025-04-16 1:17 PM
@LouisB, I think PSpectrum means to add FlexButtons to radio groups.
Just tried it now.
I can't "RadioButtonGroup::add()" using a toggle FlexButton.
2025-04-23 10:58 AM
@GaetanGodart, could I suggest to add a radio "trigger" in FlexButtons?
That way it could be managed by the base class generator.
2025-04-24 1:48 AM
Hello @Marc_LM ,
I don't think that adding a radio trigger to the flexButton would be a good thing.
The flexButton is meant to be use as a standard button but with a more customizable appearance while the radio button has to have 4 different images and each radio button is linked to another.
When changing the trigger type of a flexButton, the number of images on the "icon" visual element is always 2 but it should be 4 for a flexButton with radio trigger and then it should also "be linked" to the other "normal" radio buttons so I don't think this is something that we will implement.
Do you have a specific case where you need a flexButton and a radioButton as one button?
Maybe we can try to find a solution together with custom code for that specific use.
Regards,
2025-04-24 7:58 AM
I don't have that issue on my end because the current style I use; Pressing is equivalent to Selected.
But I do see the point that full implementation would require *RadioStyle for Text, Image and Icons.
I added my modifications to the library here for posterity.
""
Do you have a specific case where you need a flexButton and a radioButton as one button?
""
I need a radio button with text.
(I can't see the zipfiles I attached)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.