2024-05-03 6:12 PM
I have a custom container that has a box inside of it with the ClickListener enabled. I am trying to setup a callback for when the box is clicked. I have the following code setup:
#include <gui_generated/containers/NavbarBase.hpp>
class Navbar : public NavbarBase
{
public:
Navbar();
virtual ~Navbar() {}
virtual void initialize();
protected:
virtual void setupMenuItem(TextArea *label, Image *icon);
virtual void tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e);
touchgfx::Callback<Navbar, const touchgfx::Box&, const touchgfx::ClickEvent&> tMenuItemCallback;
};#include <gui/containers/Navbar.hpp>
Navbar::Navbar() : tMenuItemCallback(this, &Navbar::tMenuItemCallbackHandler) {
}
/**
* Adjusts the menu label's X position to be centered with the icon and
* adjusts the Y position to be centered with the space below the icon.
* Disabled touch interaction on both elements.
*/
void Navbar::setupMenuItem(TextArea *label, Image *icon) {
uint16_t labelAdjustedX = icon->getX() + (icon->getWidth() / 2) - (label->getTextWidth() / 2);
label->setX(labelAdjustedX);
uint16_t iconBaseY = icon->getY() + icon->getHeight();
uint16_t labelYPadding = (this->getHeight() - iconBaseY - label->getTextHeight()) / 2;
label->setY(iconBaseY + labelYPadding);
label->setTouchable(false);
icon->setTouchable(false);
}
void Navbar::tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e) {
this->DMenuIcon.setVisible(false);
}
void DMEModeNavbar::initialize()
{
NavbarBase::initialize();
// Adjust the positions of the text
this->setupMenuItem(&this->TMenuLabel, &this->TMenuIcon);
this->setupMenuItem(&this->DMenuLabel, &this->DMenuIcon);
this->setupMenuItem(&this->VMenuLabel, &this->VMenuIcon);
this->TMenuSelector.setTouchable(true);
this->TMenuSelector.setClickAction(this->tMenuItemCallback);
}
When TMenuSelector is clicked, DMenuIcon should disappear, however, nothing happens. I have looked through a variety of similar posts and code and I do not see what is going wrong here. Any direction would be appreciated.
2024-05-03 7:03 PM
Small update: I added a button widget to the project to see how it is configured, when I tapped on the rectangle first and then the button, the rectangle callback would execute...not sure why this is delayed until the button (which was not connected to anything) was clicked...
2024-05-03 11:27 PM
Hello
Try to invalidate() after set visible false:
void Navbar::tMenuItemCallbackHandler(const touchgfx::Box &box, const touchgfx::ClickEvent &e)
{
this->DMenuIcon.setVisible(false);
this->DMenuIcon.invalidate();
}About ClickListener, here is good example for box object
https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/mixins
Hope this helps !
Br JTP
2024-06-26 2:11 AM
Hello @jackcampbell ,
Have you tried the solution our amazing friend mentioned?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.