2024-06-20 11:59 PM - edited 2024-06-21 5:26 AM
I am trying to build an application on Touch GFX platform.
One of my requirement is to update project via OTA.
For that I have tried several things below.
My understanding says that I have to upload bin in MCU memory and External flash for images.
Is it possible to update touchgfx project which is in external ospi memory via custom bootloader.
Also I have to flash.hex via custom bootloader, is there any function or api to decode.hex ?
I have flashed .bin file via custom bootloader which is working fine.
But touchgfx does not generate .bin file, that why I have to decode .hex file.
Can you suggest me some standard process for OTA for specifically Touch GFX projects
2024-06-25 8:51 AM
Hello @Tech_enthusiast_Manoj,
For exemple this line generate a bin from an object file :
arm-none-eabi-objcopy.exe -O binary ./STM32CubeIDE/Debug/Application/User/generated/Texts.o blabla.bin
But then you will need to the address of that bin for flashing.
Regards,
2024-06-25 9:03 AM
Had Deja Vu there for a second..
"The format is simple and well documented, one of your coders will have to code
Perhaps use objcopy or objdump to get to a binary."
If you have the files on an MicroSD card you can read them like you would files on a PC with FATFS, FILE-X, or whatever.
.HEX tend to be about 2.5x bigger than equivalent .BIN files.
SRECORDS might also be a project worth reviewing if unfamiliar with reading files and parsing lines.
2024-06-25 9:51 PM
I know that .hex file is well documented , all the data is followed by it address.
but i need a standard code to write the correct data in correct location.
Please suggest me some standard API to do all this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.