2023-04-17 11:26 PM
Use touchgfx example with stm32f429 discovery Keil with st link usb
When I download it with 2 wire (swd), I get the message cannot load flash programming algorithm. Is there a solution?
(It is the same even if you change the debug option 0x10000000 or 0x20000000. Please help)
2023-04-17 11:32 PM
Can't load it because why?
Can't find it?
Too large to fit in memory?
The wrong one?
Needs more than one for different memory?
Needs Single or Dual bank?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.