STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I'm implementing TouchGFX on a Custom BoardI detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work.

I'm implementing TouchGFX on a Custom Board using the same circuit as the STM32H735G-DK for the external memories. I detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work. The display is always grey as the framebuffer is not writt...

MLuis.1 by Associate III
  • 1621 Views
  • 2 replies
  • 0 kudos

STM32H7 with TouchGFX __libc_init_array hardfault

Hi, i'm using STM32H750VB and it has 128kB embedded flash, so i'm using an external 16MB qspi flash. When i'm trying to fit firmware to internal & external flash, i modified linker script like this: base hal libraries are located in internal flash an...

Eralp by Associate III
  • 4947 Views
  • 8 replies
  • 0 kudos

Bare metal DMA2D

Hello allI have a custom STM32L496RGTx-based board onto which I'm migrating a legacy rendering engine. I'd really like to accelerate text rendering and I'm looking into DMA2D for a4 format font data.I have a little test setup which attempts to popula...

DCarr.1 by Senior
  • 3571 Views
  • 5 replies
  • 0 kudos

AnimatedImage can not work

I add three AnimatedImages in a screen, but only one can work normal.I transplant 'Knight Hits Zombie Game' code and bring my own project, the Zombie and Head AnimatedImages can not play but the Knight AnimatedImage work normal. (The Zombie and Head ...

V.H by Senior
  • 8967 Views
  • 18 replies
  • 0 kudos

cannot load flash programming algorithm !

Use touchgfx example with stm32f429 discovery Keil with st link usbWhen I download it with 2 wire (swd), I get the message cannot load flash programming algorithm. Is there a solution?(It is the same even if you change the debug option 0x10000000 or ...

Nhor.1 by Associate II
  • 2449 Views
  • 1 replies
  • 0 kudos

TouchGFX hangs in _exit()-function in syscalls.c

Hello there!I use a STM32F429 together with an ILI9341 based TFTLCD. I have configured TouchGFX with a partial framebuffer and it works without problems.However, the program sometimes randomly hangs in the _exit() function in syscalls.c.The cause is ...

0693W00000NrcKqQAJ.png
MAu by Associate II
  • 2919 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFx generated project gets messed up by IDE after ioc modification and code regen ('TouchINT' undeclared and other errors)

Steps to reproduce:generate project in TouchGFXopen in IDE, it compilesopen IOC, enable interrupt for uart1, save, accept the code generation (it asks about migrating code, not sure why, I have latest versions IDE 1.12.0 and GFX 4.21.3, I chose to mi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.