STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX build errors

I am new to MCUs in general and now I am working with a riverdi rvt70hssfwca0. My issue atm is that I am trying to run the stimulator on TouchGFX before I can further work on the main issue but it showing the following errors:while there is no buildi...

TTH_1-1739957506856.png
TTH by Associate II
  • 2374 Views
  • 6 replies
  • 1 kudos

Resolved! Passing references from screen to model

Hi, I was curious on the operation of the tearDownScreen function in regards to local variables created in the screen views hpp file. If I create a Struct A in screenview, and pass it by reference to the presenter then to the model, is this recommend...

Priyank by Senior
  • 2342 Views
  • 6 replies
  • 0 kudos

BW (1 bit) mode can't place pictures

I'm working with TouchGFX in 1-bit mode with custom SPI display and its working ok, but, I'm encountering an issue where any image widget I add always appears black, regardless of how I configure the PNG or try different combinations. I’ve seen someo...

Resolved! Issue with USB implementation with touchgfx

 I am using the STM32HUB50xBT6 development kit with TouchGFX. When enabling USB as Full-Speed (FS) and programming it with `USBH_PROCESS_STACK_SIZE` set to 4096, I face an issue where the allocation of `MSC_Handle` fails in the lower layers of the `u...

naveen by Associate III
  • 1069 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.