2025-03-05 2:51 AM
I am using the STM32HUB50xBT6 development kit with TouchGFX. When enabling USB as Full-Speed (FS) and programming it with `USBH_PROCESS_STACK_SIZE` set to 4096, I face an issue where the allocation of `MSC_Handle` fails in the lower layers of the `usbh_msc` file. The debugging print message shows "cannot allocate memory for MSC handle," and this occurs within the `USBH_MSC_InterfaceInit()` function.
Can anyone help me in this
Thanking you in advance.
Solved! Go to Solution.
2025-03-05 5:00 AM
this issue got solved, the problem is dynamic memory allocation when i peek inside a API of a driver there they are using malloc function to create a instant memory.
CORRECT ME IF IAM WRONG HERE:
"what i learned from touchgfx, touchgfx will not support dymanic memory allocation it only supports static allocation. " correct me here please
the same problem someone has faced. solution got explain by @Pavel A. also iam pasting the link here for reference of their conversation " Concern on the usage of malloc() on USB Host MSC ... - STMicroelectronics Community "
thank your support!!
2025-03-05 5:00 AM
this issue got solved, the problem is dynamic memory allocation when i peek inside a API of a driver there they are using malloc function to create a instant memory.
CORRECT ME IF IAM WRONG HERE:
"what i learned from touchgfx, touchgfx will not support dymanic memory allocation it only supports static allocation. " correct me here please
the same problem someone has faced. solution got explain by @Pavel A. also iam pasting the link here for reference of their conversation " Concern on the usage of malloc() on USB Host MSC ... - STMicroelectronics Community "
thank your support!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.