cancel
Showing results for 
Search instead for 
Did you mean: 

SVG vertical gradient rendered horizonally in landscape mode

Attached SVG image with vertical gradient renders correctly in TouchGFX Designer 4.24.1, but not in the simulator.
In simulator the gradient is horizontal in landscape mode and vertical in portrait mode.

Edit. SVG attachments are banned, but renaming it to TXT is banned too so my attachment wasn't attached.

"The attachment's gradient.svg.txt content type (text/plain) does not match its file extension and has been removed."

So I've attached it as source code:

<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<!DOCTYPE svg PUBLIC "-//W3C//DTD SVG 1.1//EN" "http://www.w3.org/Graphics/SVG/1.1/DTD/svg11.dtd">
<svg width="400" height="100"  xmlns="http://www.w3.org/2000/svg" xmlns:xlink="http://www.w3.org/1999/xlink">
  <defs>
    <linearGradient id="grad1" x1="0%" y1="0%" x2="0%" y2="100%">
      <stop offset="0%" stop-color="yellow" />
      <stop offset="50%" stop-color="green" />
      <stop offset="100%" stop-color="red" />
    </linearGradient>
  </defs>
  <rect width="200" height="100" x="10" y="10" fill="url(#grad1)"/>
</svg>

 

 

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
1 ACCEPTED SOLUTION

Accepted Solutions
GaetanGodart
ST Employee

Hello @unsigned_char_array ,

 

TouchGFX 4.25.0 fixes the issue.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

View solution in original post

4 REPLIES 4
GaetanGodart
ST Employee

Hello @unsigned_char_array ,

 

We are currently working on a similar issue  with SVG which might be related to your or be the same issue.
I will keep you updated once we fix it.

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
GaetanGodart
ST Employee

Hello @unsigned_char_array ,

 

Just to keep you updated, we have spotted some bugs with SVG and are fixing them.
Your issue should be part of them, I don't know exactly when it will be fixed but it will happen! :)

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
GaetanGodart
ST Employee

Hello @unsigned_char_array ,

 

TouchGFX 4.25.0 fixes the issue.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

@GaetanGodart wrote:

TouchGFX 4.25.0 fixes the issue.


Confirmed. Tested with a devboard and simulator. Both landscape and portrait render properly.

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.