STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

emWin and How to use Window as canvas

Posted on October 13, 2014 at 12:24Hello, Is it possible to use window in STemWin as canvas? I mean this - I have two window on display. One is on background and the other is above it. The second is state window - there are showed system information...

STM32F407 with SSD1963 7'' (800x480) Display

Posted on June 20, 2014 at 07:18Hi, i am working with SSD1963 7''TFT(800x480) with stm32f407 168 MHz discovery board, SSD1963 driver work fine initializing data bus and control pin as GPIO, but with slow response on TFT, right now refresh rate that ...

DCMI ov2640 JPEG, not working

Posted on September 17, 2013 at 04:35 Hello All, I've been working with the ov2640 example. I'm 95% sure I can get QQVGA out of the camera just fine; however, when I run through the registers for Jpeg I never get anything sensible out of the...

How to replace icon on STM32 Demonstartion Builder

Posted on August 12, 2014 at 22:30Hi:I am using STM3221G-EVAL board, with the demosntration builder firmware.There are multiple icons on the initial screen, and I would like to replace one of those, with one of my own icons. I have tried emWin BmpCv...

eduardo2 by Associate II
  • 4209 Views
  • 14 replies
  • 0 kudos

Camera interface firmware size in SRAM

Posted on August 01, 2014 at 13:45Sir,     I want to interface camera module that gives throughput of 28Mbps, & I want to interface it to STM32F207. The same data is to be sent to wifi module using USB 2.0 by making STM32F207 as a host. For this I ...

STemWin BUTTON_SetText() made hardfault

Posted on August 07, 2014 at 09:58Hello,when i call BUTTON_SetText() hard fault error occured. What is the possible reason? I can create button. I can write messages on screen but i cannot set button name.  #stemwin #stemwin

STM32F427VI + STemWin + RA8875

Posted on August 06, 2014 at 11:49Hello, I have a problem for driving LCD. Let me tell you about hardware first:- I am using STM32F427VI, - I am using FMC for communicating. D0..D15 and A16 and NE1 pins.- Pin connections made for 8080 mode.- I am no...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.