2014-10-13 3:24 AM
Hello,
Is it possible to use window in STemWin as canvas? I mean this - I have two window on display. One is on background and the other is above it. The second is state window - there are showed system information as needed. There is access from two tasks. The first one is window, which would be used as canvas. A few of user task can draw simple graphics objects - line, rectangle, circle, text. Sometimes user draw is made in the second window. I have configured STemWin for work as multitasking. I was looking for some function, which select window where I want to draw, but I did not find it. Can you somebody tell me, what is the right way? Thank you for help. Jiri #stm32f439-stemwinWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.