STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Store TouchGFX images to SD card

Hi,I would like to store the resources (images) to SD card. I tired storing the images to SD card as .bin file instead of images. I could successfully read the .bin file and store those contents in flash location. By this way, I could successfully di...

Iswarya by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

Can *any* of ST's "CubeMX" products produce a working STemWin project for the STM32F429DISCOVERY board?

I've been trying, on and off, for years to get a STemWin application up and running using any of ST's "CubeMX" products to create the project from scratch. I've never had any luck. I've always thought that I've been doing something wrong, but I'm slo...

Callback example for Scroll Wheel

Is there an example of how to specify and use the callback ​functions for the Scroll Wheel? And how can I get the currently selected item, if not via the callback. I found getSelectedItem() in the documentation, but it seems to be protected.

KKark by Associate II
  • 1702 Views
  • 2 replies
  • 0 kudos

Resolved! Is it possible to use the LTDC's L8 mode with TouchGFX?

Hi, I'm new here and I'm starting to develop an application on STM32H750 with TouchGFX. I've read about the STM32 LTDC's L8 (8-bit luminance or CLUT) mode. This would give a palette of 256 colors which is more than enough, and use very little memory....

sdk77 by Associate
  • 1265 Views
  • 1 replies
  • 0 kudos

I cannot get the Keil target to build without errors.

I am using the STM32F469I Disco board.I have created a project and then opened the generated Keil project. I simply try to build the generated project. The errors appear to be caused by not linking to the 'stm32f469xx.h' file. The correct compiler #d...

Matt3 by Associate II
  • 4335 Views
  • 4 replies
  • 0 kudos

Why does it say member function not declared.

Hi,I have been leaning how to use TouchGFX with the STM32F429I Discovery Board. I have managed to get buttons to work with hardware and for it to call Virtual function to toggle GPIO pins. however when i have tried to add a virtual function with a sl...

MikeP by Senior
  • 2573 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.