2019-05-06 4:55 PM
Title says it all really - just enabled hardware jpeg decode and I've lost my last mem2mem DMA channel. Various image manipulations (creating BMP file from camera image for example) requires moving a lot of data about for which up to now I've used mem2mem DMA.
Is there a mode I can put the DMA2D engine into to use it as a straight forward byte copy. I'm struggling to get past the alpha channel and windowing at present!!
2019-05-06 11:07 PM
Do You really need all streams (not channels on F7) of DMA "simultaneously"? If no, then I have to ask a silly question - do You know that one can disable-reconfigure-enable DMA stream at run-time when needed?
P.S. Physically "simultaneous" access to the same memory/bus isn't possible anyway.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.