2019-04-29 3:41 AM
Hi,
I have been leaning how to use TouchGFX with the STM32F429I Discovery Board. I have managed to get buttons to work with hardware and for it to call Virtual function to toggle GPIO pins. however when i have tried to add a virtual function with a slider i get a build error that i haven't declared the member function in the class:
no 'void Screen1View::desiredValueChanged(int)' member function declared in class 'Screen1View'
Screen1view.hpp
#ifndef SCREEN1_VIEW_HPP
#define SCREEN1_VIEW_HPP
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
class Screen1View : public Screen1ViewBase
{
public:
Screen1View();
virtual ~Screen1View() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void LED_On();
virtual void TLED_On();
virtual void desiredValueChanged(int value);
protected:
};
#endif // SCREEN1_VIEW_HPPScreen1View.cpp
#include <gui/screen1_screen/Screen1View.hpp>
#include "main.h"
#include "FreeRTOS.h"
#include "task.h"
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::LED_On()
{
HAL_GPIO_WritePin(MIKELED_GPIO_Port,MIKELED_Pin,GPIO_PIN_SET);
vTaskDelay(50);
HAL_GPIO_WritePin(MIKELED_GPIO_Port,MIKELED_Pin,GPIO_PIN_RESET);
vTaskDelay(50);
}
void Screen1View::TLED_On()
{
HAL_GPIO_TogglePin(MIKELED_GPIO_Port,MIKELED_Pin);
}
void Screen1View::desiredValueChanged(int value)
{
HAL_GPIO_WritePin(MIKELED_GPIO_Port,MIKELED_Pin,GPIO_PIN_SET);
}
Any help would be appreciated
i can upload my project if requested.
Kind Regards,
Mike
2019-04-30 1:29 AM
Hi Mike,
Please share your project. Thanks!
2019-04-30 2:13 AM
2019-04-30 2:21 AM
It's working fine here using gcc - Which compiler are you using?
Additional observation: It's generally not best practice to call your BSP (LED_On, etc) directly from your view. Let the view make a call to the presenter and then to the model or some other class which handles that kind of logic. Views should be clean (gui code only) and portable (#include "FreeRTOS.h" will cause a compiler error if you're building a simulator)
Best regards,
Martin
2019-04-30 2:29 AM
I can't really see why this wouldn't work on any compiler - Maybe you forgot to save your headerfile before compiling.
2019-04-30 5:21 AM
Hi Martin,
Thank you for your reply!
i have managed to resolve the issue by changing the default name of the slider1
I am using Atollic TrueStudio, which compiler do you recommended? I would have chosen to use Keil however there is a file size limitation on the free version for the F4 series.
Kind Regards,
Mike
2019-05-01 12:59 AM
Hi @MikeP,
Glad you solved it.
Atollic should be fine. We do not recommend anything specifically - I was just curious because they may behave differently. Keil/IAR are probably among the most used compilers commercially.
2019-05-01 1:42 AM
Thank you for your help!
2019-05-01 9:18 AM
Hi @Martin KJELDSEN
With the TouchGFX not loading the Simulator - Would you be able to expand on your additional observation mentioned earlier?
i understand that i cant have #include "FreeRTOS.h" ,#include "main.h" and #include "task.h" in my Screen1Vew.cpp but i'm unsure how i go about avoiding this. i could create separate threads and usexTaskNotifyWait and xTaskNotify but they require the "task.h"
Kind Regards,
Mike
2019-05-03 1:32 AM
Hi @MikeP,
Sure. What i meant by that is that if you're running in a simulator environment, your compiler will fail because it does not know FreeRTOS. Generally, if you have target specific code and you still wish to be able to compile a simulator, you would sorround that target specific (maybe FreeRTOS task related) block with #ifndef SIMULATOR.
The second part is, it's better to have this in the model. The model is what's being ticked globally - If you receive a tick inside your concrete view then it would be for that view only. You want to define your RTOS task interoperability (e.g. Checking queues for new messages) inside the Model::tick() method which gets called regardless of application state.
So, all in all:
Hope that helps!
Best regards,
Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.