STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

LinkerScript for STM32F7508x(gcc)

Hi.​I make TouchGFX project for STM32F7508-DK.​I want to compile with TrueSTUDIO.​I found LinkerScript file in project/gcc folder.​​This file name is ​STM32F7508x_FLASH.ld. but this file is STM32F746NGHx.​Refer to the attached file.​Please, tell me ...

SPark.7 by Associate
  • 1493 Views
  • 2 replies
  • 0 kudos

Resolved! How to insert a newline in a text area via coding

i have this problem, in my app i have a text area which say: current option:Option Ausing touchGFX i set an interaction when a button is pressed to chage that text area, and i need it to become:current option:Option Bwhen i put those tho line in the ...

0690X000008AiRxQAK.png 0690X000008AiS7QAK.png
Zui by Senior
  • 3885 Views
  • 7 replies
  • 0 kudos

Resolved! Can't load "BIG" application on STM32H750DISCOVERY board

When i try to load an application to that disco board i keep having: An error occured during flash. Please make sure you have the right target connected.STM32CubeProgrammer is placed in Program FilesSTM32CubeProgrammer is placed in Program FilesConve...

Zui by Senior
  • 2410 Views
  • 8 replies
  • 0 kudos

Support for the next 3 weeks

Hi everyone,I'll be out for three weeks for summer vacation here in Europe. In the meantime, my colleague @Anders Nedergaard PETERSEN​ will be helping you with any issues you're having.Edit: See you soon! (Thanks to @hansd56​ for pointing out that it...

How to configure properly a LCD screen?

Hello,I'm having difficulties setting up the LTDC properties in the HW_Init.cpp file for my specific LCD screen and thought that someone here could potentially help me. The lines I have to configure are the followings:hltdc.Init.HorizontalSync = 20; ...

0690X000009YjAZQA0.png
GMeur by Senior II
  • 862 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.