STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Relocating frame buffer to internal SRAM

Posted on August 07, 2017 at 11:54Hello everyone,I am attempting to relocate the frame buffer of the 'STemWin_HelloWorld' supplied with the STM32F429 Discovery kit. I would like to use the internal SRAM instead of the external SDRAM. Our project onl...

Resolved! TouchGFX .gitignore

Hello,I want to use my project under git version control,so, my question is what should I control from TouchGFX folder of my project, and what should I add to .gitignore file?Thank you,Anton

qqAnton by Senior
  • 2399 Views
  • 1 replies
  • 2 kudos

My update wishlist

If you guys are working on a new version update anytime soon, here are some things I'd like to see.Add standard shortcut keys to the top menu (Alf-F, Alt-E, Alt-H)When creating a new application, use a standard File dialog for the Application Directo...

Michael B by Associate III
  • 1054 Views
  • 1 replies
  • 0 kudos

Linker issues while compiling with IAR

We are using STM32F429I eval board and developing GUI based application using TouchGFX(Ver.4.9.3) and IAR(Ver.7.4).We are facing linking error in IAR mentioned below,Problem:  Error[Lp011]: section placement failed unable to allocate space for sectio...

NMath.0 by Associate
  • 3474 Views
  • 4 replies
  • 0 kudos

disabling the LTDC

Hi,I have my ownPCB with the STM32F429, SDRAM, TFT and others. To avoid screen flickering, I amdisabling the clock for LTDC for a time when content is changing.  If I do it very often (10 times per second) itcould happen that the MCU crash. It doesn’...

KTarc by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.