STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX v4.22.1 Language Exclusion

Hello All,I am using touchGFX v4.22.1, is it possible to exclude languages when generating a build?I have 6-7 different languages but i am close to my flash limit when building in STM32CubeIDE.I'd like to create multiple builds with different languag...

H7R7 CUBEIDE project generate touchgfx error

I want to make a project using h7r7 and enable touchgfx,In CUBEIDE,I chose both boot project and application project,but I can not check touchgfx for application project,and it is forcely checked for boot project,can't be changed.Any one knows this p...

20250525231950.png 20250525232016.png
amb by Senior
  • 1162 Views
  • 2 replies
  • 0 kudos

Resolved! what is nemagfx_stencil_buffer_mem?

I have a custom board using u599 and touchgfx, my LCD size is 640*480.I noticed there is a "nemagfx_stencil_buffer_mem" in my RAM,It takes 305K memory,It's really a lot memory ,because I only have 30K left.But on the other board,lcd size is 480*480,"...

QQ20250425-124013.png
amb by Senior
  • 1159 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.