STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touch Panel 7inch can't run with TouchGFX

I have make a customize Board using STM32F746 base on STM32F746-Disco board. but i'm using TFT 7inch with capacitor touch panel using IC FT5425.I have tested with touch panel base on example in BSP folder of STM32Cube. it run normaly. that mean FT524...

HAnh by Associate III
  • 1406 Views
  • 1 replies
  • 0 kudos

Resolved! Display Refresh

Hello,I have an STM32F469NI display board. The program I wrote runs without errors. The only problem: The display now has to update itself automatically.Can you help me with the settings I need to make? Or do I have to generate that in the code?I wou...

HSchl.1 by Associate II
  • 3678 Views
  • 6 replies
  • 0 kudos

Resolved! Issues with TouchGFX 4.13

Hi @Martin KJELDSEN​ First of all I wish you a happy new year. I hope you started well in the new yearI've updated TouchGFX from 4.12.3 to 4.13.0 and I have the following issues:The TouchGFX Generator changes the slashes from \ to / in the paths (e.g...

Marco.R by Senior
  • 3219 Views
  • 10 replies
  • 0 kudos

Resolved! from 24 to 16bit

HelloI use STM32F769I-DISCO.Does changing from 24bit to 16bit reduce the load on the CPU?What is 16bit, if 24bit is 100%?Also, can't TouchGFX change 24bit to 16bit?Thank you.

Ebun.1 by Senior
  • 1968 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.