STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Import Project selection grayed out

I opened an old project that uses TouchGFX and was told I should migrate to a newer version of STM32CubeMX. So I installed 5.6.0 and tried to do an import as directed. BUT the Import Project... selection is grayed out. Now what?

RWeil.1 by Associate II
  • 1297 Views
  • 1 replies
  • 0 kudos

Resolved! touch designer Interface with computer

Now we have a problem, our stm32 device board is delayed.Now we only can develop our UI on touch designer simulator. But we want to test our software of communication layer, using the serial port or TCP/IP port in one computer with the same port in a...

Breeze1 by Associate III
  • 1817 Views
  • 2 replies
  • 0 kudos

Problem with Vsync shifting after some

Hello,I’m working with custom stm32f429 board to drive a 7�? tft 800x480 lcd using ltdc driver, I’ve configured ltdc for showing just a blue background stored in internal frame buffer...pixel frequency is 33.4 mhz,page is shown successfully but there...

MHaji.1 by Senior
  • 1283 Views
  • 3 replies
  • 0 kudos

How can I debug problems related to TouchGFX?

I've ported TouchGFX on custom HW, but it doesn't work (I created class related from HAL, initialized TouchGFX and executed taskEntry().It is done in the next way:static LCD4bpp oled; static TAPI_Btn_c btnCtrl(keys); static NoDMA ...

SGonc.1 by Associate
  • 840 Views
  • 1 replies
  • 0 kudos

When we can see good, workable library for H743?

Hello!I heared, that touchgfx library for H743 is under construction, that working on this library is in progress.Is it really?I try to create project for STM32H743BI by CubeMX and TOuchGFX Designer. But it not starts - I see startscreen with widjets...

EEuge by Senior
  • 1381 Views
  • 3 replies
  • 0 kudos

STM32F746 Custom With TFT 7inch

I had make STM32F746 board with TFT 7inch base on STM32F746-Disco for my project.i tried to program sample file "application-std" from STM. it show 1/2 screen (272x480), that mean my PCB run normal.But my screen is 480x800 (7inch). how to i config ST...

HAnh by Associate III
  • 1482 Views
  • 2 replies
  • 0 kudos

[SOLVED] -- display large characters ---

I need to display large characters to show the dB of attenuation of my preampl.I have found a good font but the BSP_LCD_DisplayStringAt and DrawChar are not able to use this font, only half of the left section of the character is print.So I have deve...

AVI format with Motion-JPEG

Hi,​Reference the Official Code from CubeMX in STM32Cube_FW_H7_V1.6.0 -> JPEG_MJPEG_VideoDecoding.And I have built the code for my own board test, but I got some error on it.When I debug the code, it always get in HardFault at StreamSize like the ima...

0693W000000UTGXQA4.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.