2020-03-25 12:46 AM
please don't recommend to buy stm32f746 board
Solved! Go to Solution.
2020-03-25 1:30 AM
There are a couple of examples in STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Projects/STM32F7508-DISCO
2020-03-25 1:30 AM
There are a couple of examples in STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Projects/STM32F7508-DISCO
2020-03-25 1:40 AM
STM32Cube_FW_F7_V1.16.0\Projects\STM32F7508-DISCO\Demonstrations\TouchGFX
2020-03-25 7:12 AM
thank you all
2020-03-25 8:20 PM
can you also give some touch screen/graphics examples, also please explain why simulation and code generation fails in touchgfx when i try to create an application with STM32F750
2020-03-25 10:44 PM
Hi,
I have also recently purchased STM32f750-DK discovery board,I have configured USB HS and USB FS both for Communication Device Class on STM32 Cube IDE.
Code is generated and Built without any Error but On debugging USB FS Port detects on My PC as Com Port but USB HS port does not detect.
can any body suggest some solution/configurations for USB HS?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.