STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Widget Avatars

I am looking into making an Avatar widget (image inside a non rectangular container).I looked at some of the the lcd.blitcopy, canvas, circles and painters and getting a bit confused where you could apply a mask to an image to only render a section o...

Marc_LM by Senior
  • 819 Views
  • 1 replies
  • 0 kudos

Resolved! Controlling PWM from UI with TouchGFX

I want to control a servo motor with the PWM and I want to have a slider on the GUI to control the position of the servo motor, So I created a TouchGFX project added the slider and the intraction to a virtual function and I generated the code I opene...

scope_nh by Associate
  • 1110 Views
  • 2 replies
  • 1 kudos

Low qspi clock frequency in ExtMem_Boot

I noticed that any example created with touchGfx for the STM32H750B-DK demo board uses the ExtMem_Boot bootLoader that uses a 400Mhz clock instead of 480Mhz, but the strangest thing is that it uses a QSPI clock of only 50Mhz, when from the memory dat...

DDi S.1 by Associate III
  • 3268 Views
  • 10 replies
  • 2 kudos

TouchGFX on STM32F769I-EVAL without RTOS

Hello everyone,I'm currently working on a project with a custom electronic board (still in development). This project includes a 1280x400 display, driven via MIPI DSI by a processor (likely an STM32F429ZG or STM32F479ZG depending on the required pin ...

Miickey by Associate II
  • 2750 Views
  • 10 replies
  • 1 kudos

multi container and one Click Handler

hiby this code click event enable for 2 Continer  and work fine    void CNTR_A_ClickHandler(const CNTR_AntenaLevel&, const touchgfx::ClickEvent& e); touchgfx::Callback<MainView, const CNTR_AntenaLevel&, const touchgfx::ClickEvent&> CNTR_A_ClickedCa...

Natali by Associate III
  • 1476 Views
  • 2 replies
  • 0 kudos

Resolved! can TouchGFX support STM32H750VBT6 ?

It have a new project with LCD(4.3' RGB:480*272) and touch panel, To drive this LCD and touch panel, i will select STM32H750VBT6 to develop , Whether can the TouchGFX support this MCU or not ?

miker by Associate III
  • 2546 Views
  • 6 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.