STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32N6570-DK Debugger

I have succesfully built and programmed a TouchGFX application to my board in release mode. When I try to use the debugger I have limited success. If in the Project Explorer I highlight the (in FSBL) line and launch the debugger and press F8 my appli...

paulbamburak_0-1740452149686.png

Resolved! X-Nucleo GFX01M1 Display Connection Problems

X-Nucleo GFX01M1 not working properly with Nucleo-64, ARM Cortex M4, STM32 L476-Serie Hi, I Got My Hands Recently On a X-Nucleo GFX01M1 and I am now struggeling to get a Proper Connection > Everything I see Is White Screen. I have Simple Code For Tes...

Paulo1114 by Associate III
  • 883 Views
  • 2 replies
  • 0 kudos

Import Touchgfx project to IAR, it can not work

Hello,I download an example GUI from Touchgfx designer, generate code and run on my STM32H735G-DK board, it works well.Then I open the .ioc of this project and generated code with EWARM, open it and build, it has no errors.When I download it to board...

lingbo_0-1749445260556.png lingbo_1-1749445261092.png lingbo_2-1749445292205.png lingbo_3-1749445309985.png
lingbo by Associate II
  • 910 Views
  • 2 replies
  • 0 kudos

Resolved! TOUCHGFX and CPU

Moved from Feedback forum - the Feedback forum is not for product questions. Hello, I have a problem with using TouchGfx, if I create a project with an STM32F429 without adding any code the compilation is ok, if I activate TouchGFX (Graphic applicat...

PSEBA.1 by Associate II
  • 4262 Views
  • 8 replies
  • 3 kudos

Resolved! Unwanted artifacts in screen object

I'm seeing "noise" in some objects drawn on the screen.  See pic... the yellow circle ("shape") should be solid yellow, but instead includes red-orange horizontal lines.  If the circles are rearranged the yellow circle can look correct, but the blue ...

LCD_noise1.jpg
SJR1 by Associate II
  • 3191 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.