2025-06-10 10:01 AM
Hello,
I was wondering how can I change the values of each child within a container? For example, I have a container with 4 slider widgets. I want to be able to set the values of each slider using a for loop. Below shows a very simplified example of what I'm trying to achieve within Screen1View.cpp. I want to use array iteration instead of setting each slider value manually because I'll eventually have more than 10 sliders in the container.
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
int presets[4] = { 5, 10, 15, 20 };
for (int i; i < 4; i++)
{
// in the container, each of the 4 slider widgets is being set to a preset value from an array
containerSliders[i].setValue(presets[i]);
}
}
While looking into this more, I saw that containers have a forEachChild public function, but I am unsure how to use GenericCallback for this use case. If this is the way to go, can a simplified example be provided?
Thanks for the help in advance!
Solved! Go to Solution.
2025-06-11 8:09 AM
Hello @tv9 ,
For only 4 children I would do it "by hand".
But for the smart way, you can look at these threads :
Regards,
2025-06-11 8:09 AM
Hello @tv9 ,
For only 4 children I would do it "by hand".
But for the smart way, you can look at these threads :
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.