STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H7 VGA signal not working

Greetings,today I tried generating a VGA hsync and vsync signal using PWM on my NUCLEO-H743ZI2. To be precise, I wanted to generate a 640x480@60Hz signal with the help of this page.I analyzed the output of the PWM using my logic analyzer and thats th...

0693W000003QyW1QAK.png 0693W000003QyW6QAK.png 0693W000003R0R3QAK.png
MWeid.2 by Associate II
  • 1012 Views
  • 0 replies
  • 0 kudos

Unhandled exception in SDL_DestroyTexture();

Hello,I've got a strange bug at times when clicking on a 'home-made' button. VS stops at SDL_DestroyTexture(framebufferTexture); and tells me there is an unhandled exception (see image) but then, when I click on 'continue' the code runs just fine and...

0693W000003QvjbQAC.png
GMeur by Senior II
  • 880 Views
  • 0 replies
  • 0 kudos

how to print custom keyboard input?

helloi use Custom Keyboard application provided with the designer and I want to convert typed characters to strings and print this with touchgfx_printfhow to do this?

M3R by Associate II
  • 1332 Views
  • 1 replies
  • 0 kudos

Command to separate the binary from .elf file

Hello @Martin KJELDSEN​ @Community member​ ,@All ALL​ We are using TouchGFX based development kit.STM32F746G-DISCOSTM32F7508-DK STM32F746G-DISCO :When we used STM32F746G-DISCO Kit, we are using following command to separate the flash and ext-flash bi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.