2020-08-13 1:36 AM
Hi @Martin KJELDSEN ,
1) Is it possible to share the source code for TouchGFX TrulyHandsfree demo ?
https://youtu.be/B8_2XtEK4wk?list=UUPmAQbY9KbHqdQ_GwUGg1bA
2) I am planning to buy STM32F469 Discovery kit for Alexa implementation. Does ST provide Audio codec, Mic etc drivers with this kit ?
Regards,
shree
2020-08-17 1:58 AM
Hello,
1) For the TrulyHandsFree demo, I'll check if it's possible to share the code and will come back to you.
2) Regarding Audio codec, Mic, drivers, please ask in the corresponding topic as it is not directly related to TouchGFX.
/Alexandre
2020-08-28 5:40 AM
Hi @Alexandre RENOUX ,
Did you check if it is possible to share the sensory demo code ?
Regards,
Shree
2020-09-07 12:25 AM
Hello,
For the demo shown on the video, most of the graphics are available trough TouchGFX Demo 1 and 2 in TouchGFX Designer. The demo you see on the video is an old one involving 3rd party code.
As for the voice recognition, this cannot be share.
Very sorry for the late answer.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.