2020-08-31 9:38 PM
Hello @Martin KJELDSEN @Community member ,@All ALL
We are using TouchGFX based development kit.
STM32F746G-DISCO :
When we used STM32F746G-DISCO Kit, we are using following command to separate the flash and ext-flash binary.
arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F746G_DISCO.elf" ExtFlash.bin;arm-none-eabi-objcopy.exe -O binary --remove-section=*Section "$ STM32F746G_DISCO.elf" Flash.bin
Above Generated binary are working fine and we are loaded using ST-LINK Utility.
STM32F7508-DK :
When we used STM32F7508-DK kit, We are using following command.
arm-none-eabi-objcopy.exe -O binary --only-section=.isr_vector --only-section=.text --only-section=.rodata --only-section=.ARM.extab --only-section=.ARM --only-section=.preinit_array --only-section=.init_array --only-section=.fini_array "$ STM32F7508-DK.elf" Flash.bin; arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F7508-DK.elf" ExtFlash.bin;
Above command will create the binary but it is not working fine.
Here, i attached both linker file for both broad, can you please guide me on this point?
Is something that i missed?
Regards,
Nikunj Patel
2020-09-01 5:50 AM
What does "but it is not working fine" mean? Anything more
/Martin
2020-09-03 4:58 AM
Hello @Martin KJELDSEN ,
It means when i used following command for STM32F7508-DK .
arm-none-eabi-objcopy.exe -O binary --only-section=.isr_vector --only-section=.text --only-section=.rodata --only-section=.ARM.extab --only-section=.ARM --only-section=.preinit_array --only-section=.init_array --only-section=.fini_array "$ STM32F7508-DK.elf" Flash.bin; arm-none-eabi-objcopy.exe -O binary --only-section=*Section "$ STM32F7508-DK.elf" ExtFlash.bin;
It is creating a Two Binary
When i load both binary using STLINK Utility using External Loader. It will not display anything on display.
Can you please guide me.
Regards,
Kaushal Patel
2020-09-03 6:04 AM
Have you tried debugging? What's the application doing, if anything?
/Martin
2020-09-03 6:09 AM
Ok, and is flash.bin viable?
Does your loader output any actionable diagnostic information? Like checksumming or hashing what it sees, and that matches the PC side copy?
Does a disassembly show expected code?
Can you run the boot loader in a debugger, and walk the transition into the QSPI image?
2020-09-06 1:27 AM
Hello my friend
Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?
Any example of a WIFI http server with stm32h7b3i-dk ???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.