STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How can I make an modal window over custom keyboard widget

I have a screen with some pictures, buttons and a custom keyboard widget. I want to show a modal window on this window. But when I do "view" on my modal window, it only covers the things defined in gfxdesigner not the custom keyboard widget. How can ...

oe2 by Associate III
  • 2688 Views
  • 4 replies
  • 0 kudos

Touchgfx Tearing Issue in STM32F412VGT6

I made touchgfx GUI with STM32F412VGT6, my LCD is 240*240. The inferface is 8080 8bit (also tried 16bit mode). I use widget , container in my UI but when I change page in swipe container, there is tearing issue in my screen. And the tearing position ...

0693W000005D0QjQAK.png
Ewen.1 by Associate II
  • 2554 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L4R9I-DISCO problem with ARGB8888 image

Hello,I am developing on STM32L4R9I-Disco, and I want to display ARGB8888 images on the round DSI display under the command of UART. For example, I send hex 'b2' to this board by uart, one image is displayed. I have succeeded some parts, but the ima...

0693W000006EF6mQAG.jpg
Hzhan.2 by Associate II
  • 2546 Views
  • 3 replies
  • 0 kudos

NUCLEO STM32F401RE work with SSD1963 and XPT2046

Hi everyone,I am taking part in a project about display and controller using TFT AT070TN92 with graphic controller SSD1963 and touch controller XPT2046.Please can give me any libary of them for STM32F401RE ?Thank you! PS: I'm not good in English.

VNguy.21 by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

LIstwheel do not work

HiI do have a resitive touch xpt2046 and a ssd1963 screen.All widgets work fine except the listwheel.When i do touch it, it become highlightet in the first row, but it do not movelistwheel_getpos return zero i do use GUI_TOUCH_Exec(); to update  whil...

hjh by Associate III
  • 789 Views
  • 0 replies
  • 0 kudos

STM32H745 gets a Hardfault error?

 I have developed touchgfx based applications in STM32H745XI devices only in Cortex-M7. It went smooth till few screens. later adding one more screen has increased the memory as belowProgram Size: Code=149192 RO-data=549672 RW-data=8968 ZI-data=15969...

Nredd.1 by Associate III
  • 2232 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.