2020-12-01 1:06 AM
I have a screen with some pictures, buttons and a custom keyboard widget. I want to show a modal window on this window.
But when I do "view" on my modal window, it only covers the things defined in gfxdesigner not the custom keyboard widget.
How can I include custom keyboard to so that it becomes part of the "main window" or is there perhaps an better / other way?
Solved! Go to Solution.
2020-12-03 6:01 PM
To move your modal to the top, simply
remove(modalElement);
add(modalElement);at the end of your setupScreen() method. This should be done after you add() your keyboard widget, if that is not done in the base class.
2020-12-02 10:51 PM
Does anyone know if it's the drawing order, I have tried to change the "add order" by moving my kybord code the the base file (I know that it will be overritten next time I generate the code for designer) but It dosent seems to do any change the keyboard is still "on-top". Mybe the keyboard itself i "modal" (I can't find anythning in the code that supports that theory).
2020-12-03 6:01 PM
To move your modal to the top, simply
remove(modalElement);
add(modalElement);at the end of your setupScreen() method. This should be done after you add() your keyboard widget, if that is not done in the base class.
2020-12-03 10:59 PM
Thanks Michael,
Works like a charm! Easy when you know how to do it, but hard do find out how to do it...
BR Ola
2020-12-04 6:52 AM
You're welcome, happy to help! You were 90% of the way there yourself with your draw-order suspicion.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.