2020-12-03 9:24 AM
Hi
I do have a resitive touch xpt2046 and a ssd1963 screen.
All widgets work fine except the listwheel.
When i do touch it, it become highlightet in the first row, but it do not move
listwheel_getpos return zero
i do use GUI_TOUCH_Exec(); to update
while (1)
{
HAL_Delay(10);
GUI_TOUCH_Exec();
GUI_Exec();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/////
case WM_NOTIFICATION_RELEASED:
// USER START (Optionally insert code for reacting on notification message)
hItem = WM_GetDialogItem(pMsg->hWin, ID_LISTWHEEL_0);
uint16_t position = LISTWHEEL_GetPos(hItem);
// position = 15 ;
LISTWHEEL_SetSel(hItem, position);
// USER END
break;
//////
where to look after the issue ...listwheel do not move ...
best regards
Hjalmar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.