STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Issues with I2C HAL in TouchGFX RTOS thread.

Hello, i see trouble with I2C HAL_I2C_Master_Transmit(&hi2c2, addr==0 ? I2C_ADDR_DACR : addr, Buff,3,5);in project with TouchGFX RTOS i have two threads. One for GUI and second is this hw I2C.On scope i see, that I2C sometimes (random) split send or ...

MM..1 by Chief III
  • 1116 Views
  • 5 replies
  • 2 kudos

The screen is white. Please help me.

Hello, I am a beginner developer who is new to STM32 with TouchGFX.I am currently trying to display the GUI configured in TouchGFX Designer on a custom board consisting of an STM32F429IGT6 MCU and IS42S16400J - 7TL SDRAM.I have completed all GPIO set...

newbiee by Associate II
  • 1091 Views
  • 6 replies
  • 0 kudos

Resolved! Touch Gfx using LTDC 2 layers

Hello I see on this link that Touch Gfx can only use a single layer from the LTDC.https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-ltdc-parallel-rgb Is there some way of using the two LTDC's layers ?,May be i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.