STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! GPU2D not available when using L8 Pixel Format

Hi, I am using an STM32U5A9ZJT with LTDC L8 buffer and cannot select GPU2D, is support for L8 being added soon?Being able to use L8 and vector fonts would be ideal for storage savings. I also noticed that the "hardware" option for vector rendering is...

PhilipC by Associate III
  • 1805 Views
  • 2 replies
  • 0 kudos

How to debug the touchGFX Engine?

On our custom board running STM32U5G7 I have set up a project using the same configurations in the .ioc file of the STM32U5G9J-DK2 but obviously with our pinout and package. The project compiles and runs, it does display correctly on the sim but ther...

ARM_and by Associate III
  • 3691 Views
  • 4 replies
  • 0 kudos

SDL2/SDL_render.h: No such file or directory

我在使用cubeide时一直报错,下面是详细的报错信息:Description Resource Path Location Typefatal error: SDL2/SDL_render.h: No such file or directory HALSDL2.hpp /llwstm32/Middlewares/ST/touchgfx/framework/include/platform/hal/simulator/sdl2 line 26 C/C++ Problemmake: *** [M...

touchGFX can't load into stm32H750ZBT6

I built a LCD driver with stm32H750ZBT6 , afliliatlister operation, touchGFX can't load into MCU with ST-LINK , the error list as follows: (remark:  i try to set as stm32CUBE IDE or CMake) stm32CUBE MX  GCC setting:  touchGFX list error message:Compi...

miker_0-1751621024796.png
miker by Associate III
  • 531 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.