STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Flickering when certain element is open

Hello,in my app I am using a listLayout that is inside a scrollable container. In that listLayout I dynamically add and remove elements based on user touch. Each element has multiple wildcards in textAreas.Functionality is ok, but when one of the ele...

Jakicaa by Associate II
  • 923 Views
  • 1 replies
  • 0 kudos

Resolved! How to remove keychar from keyboard keys?

Hi,I,m looking for a way to remove or hide the keychar of the keyboard's keys or button, i'm using the custom keyboard from TouchGFX demo or examples, and i have a new asset that already have the keychar or key label. For this reason, i need to remov...

H_Drx by Associate II
  • 837 Views
  • 3 replies
  • 1 kudos

Resolved! Screen Not Display every widgets

Hi all,Please help to point me where I did a wrong.  I have different widget on the main screen, and when I switched back and forth, the main screen (where there are most widgets implemented) intermittently not display all the widgets.  Sometime I go...

Jtron11_0-1753734870820.png

Resolved! STM32H745I-Disco TouchGFX nothing shows on screen

Hi everyone. I have a STM32H745I-Disco board and I am using both TouchGFX and CubeIDE to make a project with the board. So the issue I am encountering is that when I wrote or made some adjustments in the both applications the project seems fine (when...

partial bitmap copy in Touchgfx

Hello everyone:I came to a need,that I need to copy part of a dynamic Bitmap to another postion of the same bitmap.I current use a for loop and memcpy func,It works but cost 4ms each run.How can I use touchgfx's blockCopy functions to do this? as DMA...

000.png
amb by Senior
  • 711 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.