2025-08-29 8:54 PM
Hello everyone:
I came to a need,that I need to copy part of a dynamic Bitmap to another postion of the same bitmap.I current use a for loop and memcpy func,It works but cost 4ms each run.How can I use touchgfx's blockCopy functions to do this? as DMA2D was already enabled.
2025-08-29 8:57 PM
I found blitCopy() func in HAL.hpp,but it seems it only use to FRAMEBUFFER.
2025-09-01 6:11 AM
Hi amb
We don't have that operation, but I think you can make one.
first call HAL::lockFrameBuffer. This will wait for the DMA to finish all operations.
call unlockFrameBuffer also.
Now, DMA2D is idle and we can use it.
Two ways:
Go to your CubeFW for the board (or another board with DMA2D and display), find the DMA2D examples.
For F746Discovery, for example this:
STM32Cube_FW_F7_V1.17.0/Projects/STM32746G-Discovery/Examples/DMA2D/DMA2D_MemToMemWithPFC/Src/
Use this code to setup DMA2D and start it.
Second:
Take the code from STM32DMA::setupDataCopy. Find the default case, marked with /* BLIT_OP_COPY */.
Use this to make a specific function for your need.
Let me know if you have questions.
Note, using DMA2D within TouchGFX requires caution. It is not recommended, unless you need to.
2025-09-01 6:41 AM
Hello:@Flemming Gram CHRISTENSEN
Thanks for your reply.I will try it.
And I have another question: the touchgfx framebuffer is RGB565,Can I make a dynamic bitmap of ARGB8888? I made one by cacheable container and display the dynamic bitmap by a texturemapper but no image came out. but if I change bitmap type to rgb565,the image can be seen. There is enough cache,I confirm the dynamic bitmap is created successfully on both type.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.