STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX Designer Installation Error

Hi Everyone,I'm trying to install TouchGFX Designer (v4.25.0) but I keep getting this error during setup:“TouchGFX Setup Error writing to file: C:\TouchGFX\4.25.0\designer\TouchGFXDesigner-4.25.0.exe. Verify that you have access to that directory.”I'...

tejo by Associate II
  • 1101 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX Designer without .ioc file

I want to use TouchGFX Designer in a Project for which no .ioc file exists, but generating code in the Designer fails because of the missing .ioc file.Is it possible to work around this? If I need to use a dummy .ioc file, which settings are relevant...

Resolved! box resize but fill colour does not change

I'm using a coloured box as a background for some dynamic text. I would like the background to match the width of the text when it changes.I can change the width of the box to match the text width, but the box's fill colour will not fill to match the...

Resolved! Proper way to synchronize with toggle button

Hi all,I am looking for an advice to how-to sync the back-end signal and the toggle button.For example toggle button by default is OFF, Signal output Low.Clicked button, the button state = ON, Signal output High.View still display the button is ON.Du...

RGB888 Configuration on STM32H750

Hi Team,   We are running into a problem on TouchGFX (v4.25) on configuring our 480x272 display on the above discovery board I mentioned. We want to configure a text box and display this  color I attached below. We found that the RGB we have is RGB56...

PushparajAdka_0-1753681159703.png PushparajAdka_1-1753681372843.png

Re: TOUCHGFX and CPU

Split from TOUCHGFX and CPU.My screen resolution is 480 * 800. When I use a dynamic graph with a capacity setting of 300 and add 30 points each time, the number of executions of handleTickEvent per second drops from 30 to 2. What solutions are there?...

Lewis233 by Associate III
  • 968 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.